EEO#.ZOFFSET

Description

Sets the position within each revolution where the Z pulse will be generated, when the one Z pulse per rev mode is selected (EEO#.ZMODE 0).

When the primary feedback position (within a revolution) equals this value, an index pulse will output.

When you are using multi-turn or single turn absolute feedback devices the Z pulse generated by the EEO will always be aligned with the same mechanical position of the of the primary feedback position. If you are using an incremental feedback deviceClosedA process whereby some proportion of the output signal of a system is passed (fed back) to the input. In automation, a device coupled to each motor to provide indication of the motor's shaft angle, for use in commutating the motor and controlling its speed and position then the origin of the primary feedback is not at the same mechanical position each time the drive powers up.

Examples

Code

To set the Z pulse to be generated at an offset of 90 degrees (1/4 turn) expressed in counts:

-->EEO1.ZOFFSET 1073741824

Context

For more information see Encoder Emulation.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units Same as FB#.P
Range 0 to 4,294,967,295
Default Value 0
Data Type Integer
See Also  
Stored in Non Volatile Memory Yes

Variants Supported

All variants are supported.